Cancel
Showing results for 
Search instead for 
Did you mean: 

Hole wizard

Not applicable
Is it just me or is the hole wizard not included in this trial version.
I'm trying the tutorial and simply can not get the hole icon in the solids section to work. This make it very difficult to gain anything from the tutorial.
3 REPLIES

Re: Hole wizard

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
It is included. When you select the Hole command, in the command bar that appears at the top of the graphics window, click the Hole Options button.


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Hole wizard

Not applicable
No, in the command bar "Home" for solids the "Hole", "Draft" and "Thin wall" as well as the what is in their drag down is "gray'ed" out.
I tried several tutorials but I get stuck when I can't use these features.
Is this a set-up problem ?

Re: Hole wizard

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Perhaps post a picture. Did you have another Solid Edge product loaded like Solid Edge 2D Free?


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com