Cancel
Showing results for 
Search instead for 
Did you mean: 

Holes dialog very slow in ST9-W7.

Valued Contributor
Valued Contributor

I have a very slow and un-rensoponsive GUI in Solid Edge ST9 on Windows7-x64, especially when creating holes. Here is a video of the application:

 

https://youtu.be/tULDfB_pcqI

 

My question is if  something is not working as expected or if this is the normal behviour of the ST9 interface.

 

I'm using a AMD Fire W5100 graphic card.

____________________________
http://www.stimarchetti.it
Design of automation
2 REPLIES

Re: Holes dialog very slow in ST9-W7.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Alessandro,

 

This actually reminds me of the issue surrounding the Windows 10 "FCU" [Fall Creators Update], so I wonder if there is an Windows update status vs. Solid Edge MP version vs. AMD graphics driver release, collaboration issue?

 

Just a thought.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Holes dialog very slow in ST9-W7.

Valued Contributor
Valued Contributor

I'm still on W7

____________________________
http://www.stimarchetti.it
Design of automation