Cancel
Showing results for 
Search instead for 
Did you mean: 

Holes in assembly.

Builder
Builder

I have a rail that has two slots in it. It is to be place on a base. Can I "transfer" the slots from the rail to the base? Any help is greatly appreciated.

 

Thanks,

D.L.B.

1 REPLY

Re: Holes in assembly.

Community Manager Community Manager
Community Manager

Several ways to do this.

 

1. If the slots are exactly identical and this is sort of a "one off" project, then you might use Assembly Features -- use the "Features" tab in Assembly and cut the slots through everything at one time. 

2. If you already have the rail and want to "copy" the slots onto the base. Then assemble them together. Then, double click on the base to edit in context. Then either do an "Include Edge" or "Interpart Copy" to get the edge or face from the rail copied over (associatively) to the base. And then just use that to cut the base.

 

DS

 

 

Dan Staples
Director, Solid Edge Product Development