Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Hotkeys for switch draft sheets up and down?

Honored Contributor
Honored Contributor

After about 100,000 hours of use. YES, it is that painful.

 

Some projects required use of those hotkeys over 500/hour

 

Unlearning something I have used over 1 million times is hard.

Highlighted

Re: Hotkeys for switch draft sheets up and down?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Re: Hotkeys for switch draft sheets up and down?

Phenom
Phenom

[quote]Maybe it would be easier to name softwares that do have this hotkey function. I don't think Acad does, Draftsight doesn't, even Excel doesn't as far as I can tell. SolidWorks, Creo, etc.?[/quote]

Just tested in autocad 2016, the hotkeys "Ctrl+PageUp" an pagedown worked perfect.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user