Cancel
Showing results for 
Search instead for 
Did you mean: 

Housekeeping No No [WHOOPS]

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi fellow edge-heads,

 

Just made a little error in judgement with my housekeeping. I was reviewing my profile on this community, and discovered there were 6 pages of images, and some were duplicated 3 times. So I thought I'd have a clean up, and diligently deleted away almost all of them, only to have a fleeting thought, just before I reaching the end....."what if they need to be there, as links to the relative posts?"

After looking at an previous post that I'd used an image on, sure enough, I'd messed up, and it now shows blank with red "X" in it.  WHOOPS!  [learnt my lesson....won't do it again...will be in the naughty corner for an hour]  Robot Embarassed

 

 

SECommunity_StudentEdition_MissingImageError.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000
2 REPLIES

Re: Housekeeping No No [WHOOPS]

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What's that they say about Experience being the harshest teacher... she gives you the test first and then teaches you the lesson Smiley LOL



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Housekeeping No No [WHOOPS]

DOH!!!

 

wONDER IF YOU PUT THEM BACK WIHT SAME FILENAMES IF THEY AUTOMAGICALLY RELINK... (Oops, Sorry for CAPS)

 

OR wonder if admin can pull from back up? 

 

Either way...   we (I)  forgive you...  Merry Christmas Sir to you and yours!