Cancel
Showing results for 
Search instead for 
Did you mean: 

How Snap Dimension or sketch in Assembly

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi;

How can I select model edge for reference Dimemsion or Sketch line. when I want create feature on Assembly?

3 REPLIES

Re: How Snap Dimension or sketch in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Famer,

 

In the case Assembly Features, especially for Frame members, I would recommend using sketch elements, with a combination of "Project to Sketch" [formerly "Include"] command and manually sketched lines/arcs to dimension from and to....as midpoint will only work for 45 degree miter cuts.

Also, check that the "Keypoints" selection filter, for your dimensions, has the correct setting. I normally just set it to "All"....I really wish this could be set as the DEFAULT.

 

2017-05-08.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: How Snap Dimension or sketch in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think you are talking about the "peers" setting in tools. It needs to be on. This is another thing I wish was always on by default.

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: How Snap Dimension or sketch in Assembly

Honored Contributor
Honored Contributor

Peers on/off is the next thing I plan to add to my quick access toolbar in every environment. I frequently have to use peer on for one side of a dimension and peers off for the other side.