Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I change the default sharpness in the Parts environment?

Creator
Creator
8 REPLIES

2 options,   SE options - View tab - Arc Smoothness   and...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

2 options,

 

SE options - View tab - Arc Smoothness

 

and on the menu View Tab - Sharpness

 

http://screencast.com/t/15yrnrb0U2

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: 2 options,   SE options - View tab - Arc Smoothness   and...

Phenom
Phenom
It'd be nice if these sharpness settings actually "stuck". Going to the View tab and the Sharpness dropdown on every. single. document....gets old.
-Dylan Gondyke

The question is WHY do you want to change it:   1. You wo...

Community Manager Community Manager
Community Manager

The question is WHY do you want to change it:

 

1. You work on really big parts (10M across) and the arcs look too faceted?

2. You work on stylized parts and you want the highlights to look more clear?

 

The answers are different, depending on what you are trying to do...

Dan Staples
Director, Solid Edge Product Development

You can change the way arcs look on the View section of t...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can change the way arcs look on the View section of the Solid Edge options.  There are two settings... An Automatic-sharpen command that is off by default which I believe is dynamic and the Arc smoothness command which I believe is static.  I believe the automatic-sharpen option overrides the Arc smoothness option.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: 2 options,   SE options - View tab - Arc Smoothness   and...

Creator
Creator
Thank you mjohnson for the reply and the screen shot. Changing the Arc Smoothness in the Solid Edge Options menu did the trick.

I agree with Chally72 that changing it in the View tab every time you get into a part is tedious.

Re: You can change the way arcs look on the View section of t...

Creator
Creator
Your answer agreed with mjohnson and worked. Thanks.

Re: The question is WHY do you want to change it:   1. You wo...

Creator
Creator
That question is so wrong on so many levels!

Why do I want to change the default sharpness of my parts? Because I paid for Solid Edge and that's the way I want it to work!

I had an 18" part with 1/2" ' holes, and the holes were 12 sided instead of round. I would change the sharpness from the default 2 to the smoother 5 and then the next time I got into that part, or any other part, it defaults back to 2. Why?

Fortunately, mjohnson's post on changing the Arc Smoothness in the Solid Edge Options menu fixed my problem.

Re: The question is WHY do you want to change it:   1. You wo...

Community Manager Community Manager
Community Manager
Wow. Didn't mean to strike a nerve. I was only asking not because its not a good question, but because there are 3 different ways and each is better suited to different situations. I was just trying to find the best one for you.

I am glad Matt's suggestion helped you.
Dan Staples
Director, Solid Edge Product Development