Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I found Files in large assembly quickly_V2

Phenom
Phenom

QUERY:

To start a Query in SE we have exatelly 13 Parameters to search for:

 

query_02.jpg

 

It could be tha case, that a company has ist own customisable Parameters like it is the case with the following situation:
-Parameter 1 : Bezeichnung1
-Parameter 2 : Bezeichnung2

 

query_04.jpg

 

To avoid wasting time in configuring a query for "every" Assembly, I propose to Copy the content of the Parameter 1 & Parameter 2 and paste them in the field: "Stichwörter" that every SE-User has access to it in the following format for example:
Content of Parameter 1 - Content of Parameter 2

 

query_03.jpg

 

During saving our files for the first time, if we Copy & Paste these Parameters in the right Filed, we could start a Query and find every Part in every Assembly easily without extra effort and time comsumption!

 

query_05.jpg

 

I am now looking for a possibility to copy the 2/N-Custom Parameters and to paste them in the Field "Stichwörter" globaly in a managed or not managed environement without the need the do it manually!

 

Thanks in advance,

Yasser

 

 

5 REPLIES

Re: How can I found Files in large assembly quickly_V2

Phenom
Phenom

From the file properties I used the following fields: 1 & 2

 

-Open the files in Solid Edge
-Click on: "Properties Manager"
-Copy & Paste the Customised information to the fields 1 & 2

 

=>Now it's possible to search for this information globaly from any Assembly without wasting time in customising a Query for each Assembly...

 

Yasser

 

query_03_Solution.jpg

Re: How can I found Files in large assembly quickly_V2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure I follow exactly.

So now you just specify "keyword" or "stichworter" in your query?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: How can I found Files in large assembly quickly_V2

Phenom
Phenom

Exactelly bshand...

 

In Solid Edge / ASM I have to search for one of the parameters, that Solid Edge offers.

 

It's not the best sollution but it helps me in the Assemblies and also in the Drafts.

 

Yasser

 

query_05_Sollution.jpg

Re: How can I found Files in large assembly quickly_V2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I didn't know you could use the Summary tab in file properties that way.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: How can I found Files in large assembly quickly_V2

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


not certain to understand You complete, but as far as I have unterstood,
there are to ways to accomplish Your needs.

 

Either use a saved query instead of the quick query (yOu can copy it from one asm to another or You write a small macro for copy one or more properties  to "Stichwörter"

 

I would recommend here to use the comment if possible, since there is the opportunity for a multiple line text.

That means evry original proerty could be in a different line.

 

I think for comparing and finding it could be easier.

 

I know, that the macro code for copy/paste proeprties form one to another field isn't that difficult,
and I think thee already exists macros doing exactly that.

 

We have to look for.

 

Maybe the forum community can help here

 

 



regards
Wolfgang