Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I have 2 or 3 decimals positions when I want to have a variable like weight in the BOM? ST5

Creator
Creator

When I try to have variables like weight in BOM, the small parts like washer or bolts are shown like 0 lbm, how can I change this variable to show 2 or 3 decimal positions?

2 REPLIES

Please see the following Help Page link and look for the...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Please see the following Help Page link and look for the "Precision" section to control the number of decimal digits.

 

http://support.industrysoftware.automation.siemens.com/training/se/106/en_US/index.html#uidSmiley Tonguerptxt4a



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: How can I have 2 or 3 decimals positions when I want to have a variable like weight in the BOM?

Creator
Creator
See also:
https://www.eng-tips.com/viewthread.cfm?qid=181215
e.g. for two decimal precision:
%{Mass/@2|R1}
(notice the order of the /@2 is before the |R1); also note only the one %.
Srypstra

ST7 MP0 | Win7