Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I pattern parts that are different heights?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

ScreenHunter 17.jpgI need some advice and I'm sure there are some lateral thinkers out there that can help?

 

I want to be able to create a truss, similar to the image above, that can be varied in length and as the length grows, the area is filled with more uprights. I have designed this in frames, but that doesn't give me the option of having varied heights. Suppression variables only work, I think, with assy features or relationships.

 

Can anyone think of a way of controlling the number of uprights as the length of the frame is changed?

5 REPLIES

Betreff: How can I pattern parts that are different heights?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alan

 

 

 

this is possible using the frame tool in ASM.

 

I remembered a similar question one year ago with a helix pattern of frames.

 

And so I would use the same method.

 

  • First create YOur place holer part with a sketch and 3D sketch patterned and splitted
  • This placeholder part again can be used for the frames in ASM
  • See video

PS.:

don't worry about the extrusion body in my master part.

This seems to be a bug in ST10 with no MP

One year ago with ST9 and in my old part it also was possible to pattern a curve only even if there is no volume present.

So the small extrusion only is a turnarround to activate the pattern command!

 

(view in My Videos)

 

regards
Wolfgang

Re: How can I pattern parts that are different heights?

Honored Contributor
Honored Contributor

Howcad is right. This is pefect for the frame tool.

Betreff: How can I pattern parts that are different heights?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hi Wolfgang
Can you attach the parts/asms for this so I can see more clearly. I'm struggling to get the pattern to work.
Thanks

Betreff: How can I pattern parts that are different heights?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alan

 

 

no matter.

 

 

regards
Wolfgang

Betreff: How can I pattern parts that are different heights?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Thanks Wolfgang. Your help has been supurb.