Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I put a retaining and snap rings on Solid Edge?

Experimenter
Experimenter
4 REPLIES 4

Re: How can I put a retaining and snap rings on Solid Edge?

Honored Contributor
Honored Contributor

Can you be more specific about the problem. Why are they not treated like any other part?

Re: How can I put a retaining and snap rings on Solid Edge?

Experimenter
Experimenter

Sorry, but I'm a beginner in ST9, so I do not know how to put a retaining ring on my assembly. Can you show me how I do?

 

 

Re: How can I put a retaining and snap rings on Solid Edge?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello are you referring to which assembly constraints should be used?  

 

Here is a model that uses a retaining ring.  It is constrained with a mate to one wall of the groove in the shaft and an axial constraint to the shaft.Snap Ring.JPG

 

If you are using an E-Clip or something that may not have a circular shape, you can always sketch a circle in the clip part itself and use it to locate the clip in the assembly.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: How can I put a retaining and snap rings on Solid Edge?

Experimenter
Experimenter

Ok, Kyle

 

Thanks for your hell.