Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I write subscripts and superscripts

Not applicable
Good evening. I have a question: is it possible to write a text label, that includes normal text and subscript? In Auto CAD it's done with an operator "^". Is such function supported at all or you should make the letters of a different size and place them where needed. Waiting for answers.

PS: Sorry for poor English.
10 REPLIES 10

Re: How can I write subscripts and superscripts

Not applicable
Superscript/subscript is not supported at this time.
Regards,
Rick B.

Re: How can I write subscripts and superscripts

Creator
Creator

Is it possible in ST8 now? I would like to write superscripts in a table.

Re: How can I write subscripts and superscripts

Experimenter
Experimenter

I cannot find a way to add super case in ST8 and ST9... I need to write annotation referring to Area size, i.e

Contact paint shall be placed on area of minimum 10.5 mm^2.

It looks like SolidEdge drawing do not exponentiation ?

 

Re: How can I write subscripts and superscripts

Experimenter
Experimenter

 

b.t.w.  Your webpage html corector is also rejecting pure html <SUP> </SUP> tag. - It performs as blind SolidEdge...

Re: How can I write subscripts and superscripts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Przemek  Superscript characters are possible in limited form for common items like "squared" and "cubed" by using the Font characters in a Font set that represent these.  You can find them via the CharMap tool and they can be typed in by pressing the ALT key and typing in their code which is displayed in the lower right.  For instance ² is ALT+0178, ³ is ALT+0179



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: How can I write subscripts and superscripts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

Hi @Przemek

 

 

You also should find them directly on keyboard using the "Alt Gr + 2" and "Alt Gr +3"

At least all of our keyboards have printed them there

 

On the other hand You can use the format functions of Solid Edge to get them.

Use the Text-Stack 

20171221_2004.PNG

 

regards
Wolfgang

Re: How can I write subscripts and superscripts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Przemek

 

 

and forgot to show the Alt Gr method as result:

 

20171221_2007.PNG

regards
Wolfgang

Re: How can I write subscripts and superscripts

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Another method would be to use MS Word if it is installed on your computer.

Type mm2, then select just the 2 and press <Ctrl><Shift><+> keys together.

This will raise the 2 and result in mm²

Now its ready to be copy-pasted to Solid Edge. 

Re: How can I write subscripts and superscripts

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Yet another method would be to use the Charmap command.

This is found on the Sketching tab of the ribbon bar in the Insert group, as shown below:

 

CharMapSE.png

Locate the ² character from the table then click the Select followed by the Copy buttons.

Now paste it in Solid Edge.

 

CharMapSQCube.png