How can it be done to move both the pattern and the Part

PLM World Member Builder PLM World Member Builder
PLM World Member Builder

I made a mistake in the assemble. How can it be done to move the pattern and the parts at the same time

Thank You

1 REPLY

Yes, you only need to redefine [or, relocate] the primary...

Esteemed Contributor
Esteemed Contributor

Yes, you only need to redefine [or, relocate] the primary part of the pattern within the assembly, then redefine the pattern sketch. [you may need to delete some of the existing constraints, in order to reposition it]

... http://screencast.com/t/YmbCTmklcVcZ 

 

If you want to use a different part instead....right click on the part in the pathfinder, go to "More", choose "Replace Part"...then choose the file to replace with...relationships will need to be redefined, and the pattern should update to use this part also. [otherwise, right click on the "Pattern" in the pathfinder, and choose "Edit", then select the new target primary part.

 

ST5_Assembly_ReplacePart.jpg

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000