Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: How can we set default layer for text, ballons & for annotation.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Dirk:

   

That is a good macro, just as what I had in mind when I offered to write a new one, though this one is quite elaborate and meticulously written.

   

A drawback I found with a simple run is - all layers from the Excecl are created even if an object of given type doesn't exist on the sheet. There is an antidote though Smiley Happy - using the Purge Layer macro on the drawing before releasing!

There is something mentioned about empty layers and deleting them (Yes/No) in the Excel though neither Google or Bing could translate it to an understandable level.

  

~Tushar

Re: How can we set default layer for text, ballons & for annotation.

Genius
Genius

Hi Tushar,

 

Sorry for all this. I will try to explain it to you. see screenshot also

Tushar if you want to delete empty layers or purge layers like you call it then you have to set the switch

"Lege layers verwijderen" = "purge empty layers" to YES.

Another thing the first column may not be changed ! But I think you already discovered this.

 

Have fun with it !!!!Smiley Happy

 

 

Dirk Rutten

Solid Edge ST6 user !!!!