Cancel
Showing results for 
Search instead for 
Did you mean: 

How delete a Study case in Simulation

Hello all,

I just have a quick question: how do I delete a old Study Case from a assembly? It is done in Simulation, but I made an error. Offcoarse I can create a new study case but I want to delete the old one.

 

Already tried to delete the .cfg file, no succes. Also tried it by deleting the .asm.ssd file, also no succes.

-------
Daniël Schuiling
4 REPLIES 4

Re: How delete a Study case in Simulation

Phenom
Phenom

Did you try right clicking the study in the Simulation edge bar and deleting (left hand side by default)? Think you can also right click the top level to delete all studies.

Re: How delete a Study case in Simulation

I cannot do that, if I do a RM click on the study case it gives me the possibility to at it to my QAT.
-------
Daniël Schuiling

Re: How delete a Study case in Simulation

Phenom
Phenom

Are you sure you're clicking on the study inside the edge bar and not on the edge bar itself?

 

Also, make sure the Simulation edge bar is not hidden by using the drop down arrow at the top of any other edge bar to enable it.

 

study.png

Re: How delete a Study case in Simulation

Ahhh, I did not had Panes for Simulation on. Thanks
-------
Daniël Schuiling