Cancel
Showing results for 
Search instead for 
Did you mean: 

How disabile perspective modification?

Pioneer
Pioneer
Hi!
Often I accidentally change the perspective view when I modelling, because I press Ctrl + shift buttons + rotate the mouse wheel.
Can I disable this shortcut or customize it with an other function?
Thanks!
14 REPLIES 14

Re: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can I ask why you frequently press control + shift in the first place?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How disabile perspective modification?

Pioneer
Pioneer
when I zoom in, out , rotate and move the model view I use the mouse wheel with Ctrl and shift button, but some time I press these buttons at the same time and when I push the mouse wheel occasionally I rotate the wheel for 1 step, and the perspective view starts

Re: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK. I sometimes use shift and the mouse to pan but I never touch control to manipulate the view. Not sure why you need to.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How disabile perspective modification?

Pioneer
Pioneer
I use Ctrl + mouse wheel press for zoom in zoom out.
I can use the right mouse button but I like mouse wheel.

Re: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ctrl+mouse wheel does nothing for me. I just rotate the mouse wheel for zooming.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Cek

 

 

 

here is my advice which I give to every trainee in my courses:

 

Use the RMB (Right Mouse Button) together with a key on keyboard (CTRL, Shift and ALT) rather than the MMB (Middle Mouse Button) which normally today is a wheel and not so easy to use.

 

If You get familiary with the RMB You wil see the advandages over MMB

Besides that it als works as well with every 2 button mouse - OK there are not so many in use but they are.

 

There is only one situation where You have to use the MMB and this is when it is to define a rotation point/axis for mouse rotation with - Yes - the RMB

 

 

 

regards
Wolfgang

Betreff: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've used the middle mouse button for zooming for years. Not sure what you mean by "advantage" of other means. With your method I have to put my coffee down before zooming. Not cool.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

the advantage I see is to not get in the problem to create perspective views.

And wether to click the MMB (wheel) or the RMB seems for me not be be that big difference.

There only is the plus, that it is no wheel only a button.

 

 

regards
Wolfgang

Betreff: How disabile perspective modification?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't get it. I only turn the mouse wheel for zoom so I never have the accidental perspective problem. In fact I never even knew about that possibility until this post.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200