Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I change the thickness of the part in sheet metal?

Builder
Builder

I've gone ahead and designed my part, and then I realized that I specced the thickness incorrectly at the beginning. Is there any way for me to edit the thickness? I tried editing it in the variable table, but it gave me an error "The edit of the feature variable cannot be applied to the model. The original value will be restored."

2 REPLIES

Hi Luke,   Sure is,....go to the Application Button / Pro...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Luke,

 

Sure is,....go to the Application Button / Properties / Material Table - "Gage" tab.

Also, if you right click on "Material Table" button, you can add it to QAT [Quick Access Toolbar] which allows you to get to this much easier.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Hi Luke,   Sure is,....go to the Application Button / Pro...

Builder
Builder
"Unable to modify material properties. Model may have dimensions or relationships established preventing modifications." Smiley Sad

I'll fiddle around with this.