Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I delete *.sev files from Solid Edge MV when installed on Ipad?

Creator
Creator
3 REPLIES

Hi David,   I've only used the Android version,....you ca...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi David,

 

I've only used the Android version,....you can add & remove your own content from the viewer, but the sample files are part of the software, which you can switch the display of these to "Show or Hide" via the options. HTH.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Yeah, you can't delete the samples, but you can hide them...

Community Manager Community Manager
Community Manager

Yeah, you can't delete the samples, but you can hide them. Go under the tools settings on the ipad and go down to SE mobile viewer and then check to hide samples.

Dan Staples
Director, Solid Edge Product Development

Re: Hi David,   I've only used the Android version,....you ca...

Creator
Creator
Thanks for the help. Just getting to grips with the app (which is really useful for site meetings).
DavidScD

Sent from my iPad