Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How do I get align the isometric view after I add the break line?

Creator
Creator

Hello all

 

In DFT drawing, I try to add a break line in a isometric view in order to reduce the long tube. but after the apply the break line, the tube doesn't get aligned.

1.png

 

thanks and regards

Hunter

4 REPLIES 4

Re: How do I get align the isometric view after I add the break line?

Valued Contributor
Valued Contributor

I have tested it.
In the iso view, it was not sorted as I wanted.

Considering the reason, the spacing is reduced in the view as it is.
The position expressed is intact.

The "split" function is thought of as a function that should be used in a flat view.

 

22.png

Betreff: How do I get align the isometric view after I add the break line?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hunter_Han

 

 

 

the only way I have found for such "breaks" is to have twice the same view (ISO), reducing the border (similar to split curve)  and then move the view accroding to the wanted result.

 

This more or less is no to much different or complex then breaking the view

 

Default breaking seems to be work  and to be created for main views only

 

regards
Wolfgang

Betreff: How do I get align the isometric view after I add the break line?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It would be a nice enhancement to be able to break iso views and maintain alignment of the components in the view.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: How do I get align the isometric view after I add the break line?

Creator
Creator

Thanks for the explaination.

it seems that's the best way to do.

 

regards Hunter