Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I set the scale of the drawing such as 1/4" = 1'

Not applicable

I can't seem to find the setting for the scale of the whole drawing. Can someone
point out to me where this setting is?
Also, are there construction template inserts such as doors, windows, sinks, etc?
Thanks for your help.
Mark B.
1 REPLY

Re: How do I set the scale of the drawing such as 1/4" = 1'

Not applicable
Mark,
Depending upon how you are creating your drawing, you have a couple of
options, both have to do with scaling the drawing border. When drawing in
Solid Edge, you always draw at full scale. Ricky Black has posted a Word doc
explaining this in depth. The post is titled "Re: Scaling large objects"
and was posted on "8/6/2007".
Since Solid Edge is a "mechanical design" product as opposed to an
"architectural design" product, you will not find architectural scales such
as you mentioned in your subject, you will have to convert it to a
mechanical scale (1:48) or a decimal scale (.0208333...).
For your "construction templates" (Blocks), you will not find the items you
mentioned because, as mentioned earlier, Solid Edge is not an architectural
design product. I believe you can use any commercially available AutoCAD
Block Library. See Help for details.
PellaKen
http://grundey.blogspot.com
"Mark Blanton" wrote in message
news:473610fa$1@bbsnotes.ugs.com...
>
> I can't seem to find the setting for the scale of the whole drawing. Can
> someone
> point out to me where this setting is?
>
> Also, are there construction template inserts such as doors, windows,
> sinks, etc?
>
> Thanks for your help.
>
> Mark B.
>