Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I shut off the annoying "Save Now" pop up in ST6?

Experimenter
Experimenter

I have auto save set up, so I don't really like being prompted to save my files. There has to be a way to shut this off, I just can't find it.

4 REPLIES

That is the Auto-Save feature... It prompts you after you...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is the Auto-Save feature... It prompts you after you complete any in process commands you are performing based on the Interval you have set when you turned it on.  If this is simply for just in case you crash, use the other option to create a backup copy.  If you crash, I believe Solid Edge will provide a prompt when you start it again asking if you want to recover from the backup.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: That is the Auto-Save feature... It prompts you after you...

Experimenter
Experimenter

Auto-save has to be renamed to 'prompt me to save' because that is pretty much what that option does. There is no Automatic saving.

 

 

Re: That is the Auto-Save feature... It prompts you after you...

Valued Contributor
Valued Contributor

If you think about this for a miniute or two, do you really want to fully automatily save everything you do ?

You could get into an almighty mess ! It's simply giving you an automatic prompt to save or not..

Geo.

Re: That is the Auto-Save feature... It prompts you after you...

Experimenter
Experimenter

Hi Geo,

Which is exactly my point about renaming that feature, so it matches it's function!

 

It is misleading to call it 'auto-save' if it does not automatically save.