Cancel
Showing results for 
Search instead for 
Did you mean: 

How do you extrude a part's face to another surface in assembly

Creator
Creator

Dear Members,

 

I have a tube to which outer surface I would like to extrude an another part flat face. All this could be done in assembly part editor? What is the easiest method?

 

Extrude to curved surface.jpg

4 REPLIES

Re: How do you extrude a part's face to another surface in assembly

Gears Phenom Gears Phenom
Gears Phenom

replace face


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: How do you extrude a part's face to another surface in assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @magiclevinho,

 

To expand on what @Johnson_BigMatt says.....from the assembly, you can Edit [or Create] in-Place, then use the "Inter-Part Copy" command to select certain reference surfaces to pull into the new PAR/PSM file, then use these for 'Replace Face" [or profile geometry location] up to the reference set selected.

 

Attached ST9 file set, is a very crude assembly [ZIP compressed file] I made, using that technique,....for your interrogation. HTH.

 

2017-03-16 (1).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: How do you extrude a part's face to another surface in assembly

Gears Phenom Gears Phenom
Gears Phenom
IIRC sync parts do not need a IPC for replace face anymore if done as an IPA. Furthermore Replace face now supports multiple "from" face selections even across multiple parts..

Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: How do you extrude a part's face to another surface in assembly

Creator
Creator

Wow! Thank You @SeanCresswell!! That's the solution!