Cancel
Showing results for 
Search instead for 
Did you mean: 

How do you remove the border around text and bitmap images

Experimenter
Experimenter

Hi all,

     I use solid edge 2d drafting for our cnc plasma table at work, and I am trying to figure out how to remove the square box /border around any text or bitmap images I use. I can't "trim" or delete it, because selecting the box selects the entire text. It treats it as one feature to remove. How can I get around this? I don't want a box around text every time I do it. Thanks,

 

icampy

12 REPLIES 12

Re: How do you remove the border around text and bitmap images

Legend
Legend

I never could find a way to do it without exporting to .dxf file, and then open and unblock the item, allowing me to remove the border. Then I would use the .dxf in the CNC software. Some CNC software already has the ability to unblock as well.

Betreff: How do you remove the border around text and bitmap images

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @icampy

 

 

this is a very easy task.

 

After selecting the textbox (and it is similar for pictures) look to the smart ribbon bar and find the icon for the "Border".

Unselect the border and the rectangle will be away, or click it again, what will show it again.

 

20170817_1452.PNG

regards
Wolfgang

Re: How do you remove the border around text and bitmap images

Gears Phenom Gears Phenom
Gears Phenom
from memory:

RMB, Properties, 2nd tab, there should be a check box to show border...

Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: How do you remove the border around text and bitmap images

Experimenter
Experimenter

I don't seem to have those options. 

Re: How do you remove the border around text and bitmap images

Experimenter
Experimenter

Re: How do you remove the border around text and bitmap images

Gears Phenom Gears Phenom
Gears Phenom

You are using a text profile from the sketching tab under insert, while the others in their answers are using plain text from the annotations. Below red arrow shows what they are using and blue is where you are.

text.PNG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: How do you remove the border around text and bitmap images

Experimenter
Experimenter

Awesome, thanks! That takes care of one half. Now I need to figure how to remove the border from a bitmap png. 

Re: How do you remove the border around text and bitmap images

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If turning off the border in the properties dialog doesn't remove the border then the border is probably part of the image itself. You'd have to edit the image and remove it.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How do you remove the border around text and bitmap images

Experimenter
Experimenter

So I got the border removed....but the .png doesn't show up in sheetcam for some reason (the text will). Any idea what settings I need to change so it will also show up in cam software?