Cancel
Showing results for 
Search instead for 
Did you mean: 

How is the best way to convert to autocad dxf files/

Not applicable
We are using free 2d to make drawings and then have to clean them up(remove dimensions, brake lines, etc.) and convert to Autocad dxf files so it will work with the preporation software for one of our machines. How is the easiest way to do that?
2 REPLIES

Re: How is the best way to convert to autocad dxf files/

Not applicable
After posting my dxf question I looked at the previous post "Dimensions automatically on their own layer...". I haven't tried it yet but it appears that this answers the question that I had about converting to autocad dxf files.

Thanks,
Chris

Re: How is the best way to convert to autocad dxf files/

Not applicable

Click on the application button in the upper left corner of the application window.
Click on 'Save As'.
In the save As dialog, change the filetype to DWG or DXF.
Save the file.
You can click on the Options button in the Save As dialog to modify the translation
options for DWG and DXF.
regards,
Rick B.