Cancel
Showing results for 
Search instead for 
Did you mean: 

How to Control Round Off With Dimensions in Solid Edge

Experimenter
Experimenter

Hey guys,

 

I'm wondering if someone can help me edit a callout containing some property text in the SE drafting environment.

 

I have placed some PMI dimensions on a part, renamed and exposed them using the variable table, and then referenced them using the 'graphic connection to part' in the property text editor.

 

I've managed to remove the "mm" from the property text (thanks to this post), now I would like to change the dimension precision/round-off, i.e. "25" instead of "25.00". I've tried chaning the round off of the actual PMI value to 1mm as opposed to .01mm, but this has no effect.

 

I can achieve the desired result by changing the file properties -> units -> precision value, but I would really like to do this with the property text instead!

 

Here's my property text formula:

%{RHS_DIM_1/CP/NU|GP} x %{RHS_DIM_2/CP/NU|GP} x %{RHS_THICKNESS/CP/NU|GP} SHS

 

And here's a few thousand words:

 

 SE_Property_Text.png

SE_PMI.png

3 REPLIES

Re: How to Control Round Off With Dimensions in Solid Edge

Genius
Genius

You'll have to change or modify the dimension style in your model. Styles - Dimension - Pick the style you are using - Modify - Units Tab - turn off the Zeros Trailing.Capture.PNG

Re: How to Control Round Off With Dimensions in Solid Edge

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

The other way to do it is to edit the callout.  The @0 changes the number of digits after the decimal point from the default of two to zero.

 

OLD:

 

%{RHS_DIM_1/CP/NU|GP} x %{RHS_DIM_2/CP/NU|GP} x %{RHS_THICKNESS/CP/NU|GP} SHS

 

NEW:

 

%{RHS_DIM_1@0/CP/NU|GP} x %{RHS_DIM_2@0/CP/NU|GP} x %{RHS_THICKNESS@0/CP/NU|GP} SHS

 

 

Re: How to Control Round Off With Dimensions in Solid Edge

Experimenter
Experimenter

Exactly what I was after,

 

Although, the @0 needs to come after the "/" like so:

 

%{RHS_DIM_1/@0CP/NU|GP}....