Cancel
Showing results for 
Search instead for 
Did you mean: 

How to Create a Pentagon with inwardly curving lines?

N/A

I'm just starting with SE ST6 and right now I'm learning to use it by creating small parts I want to place inside a tool box with a foam insert. So far I was able to create a very basic tool I use and was even able to add a threaded M8 hole. Now I am moving on to the screw knob and matches that tool that has a M8 threaded bolt and a 5 pointed "star" type knob.

I've attached a photo, the knob I am trying to recreate in SE is "B" the one in the middle.

I would appreciate any help in choosing the right tool and sequence within SE to create the part. I have searched Google and even youtube but I may not be using the right keywords to find what I'm looking for exactly.

2 REPLIES

Re: How to Create a Pentagon with inwardly curving lines?

N/A
just one possible approach of many...

http://screencast.com/t/96FozjnX0Y

HTH

Re: How to Create a Pentagon with inwardly curving lines?

N/A
wow. I should have seen that!!! I was using the polygon tool but just didn't think of using it as references for additional lines!
Thank you for taking the time to make that video. :-)