Cancel
Showing results for 
Search instead for 
Did you mean: 

How to Install JT2Go 10 and Solid Edge ST 6 at the same Computer with no conflicts and crashes?

Valued Contributor
Valued Contributor

Hi there,

I have installed Solid Edge ST 6 at my PC and after successfully testing the main functions Solid Edge ST6, Solid Edge Viewer and View and Markup I installed JT2Go in Version 10.1.

After the first start of JT2Go 10 .1, crashed always at opening from a 3D Part, ASM, JT, VFZ, VF and so on, Solid Edge Viewer and View and Markup, only Solid Edge ST 6 runs than and JT2Go.

Please Help me.

3 REPLIES

Re: How to Install JT2Go 10 and Solid Edge ST 6 at the same Computer with no conflicts and crashes?

Valued Contributor
Valued Contributor

Here is an answer from UGS, but this is only included up to Solid Edge 7.

With Solid Edge 8 the *.bat does not help anymore with this existing problems.

 

UGAnswer:
By executing the following steps the necessary registry values for Solid Edge
will be reset:

1. Login with local administrator priviledges
2. Set User Access Control to lowest level
3. For Solid Edge 32bit Version:
    cmd: cd c:\Program Files\Solid Edge ST7\Program\PLMVis  
or for Solid Edge 64bit Version:
    cmd: cd c:\Program Files\Solid Edge ST7\Program\win32\PLMVis
4. iSeriesInstall.bat

 

Hope it needs not another year to get an better answer.

 

 

Re: How to Install JT2Go 10 and Solid Edge ST 6 at the same Computer with no conflicts and crashes?

Gears Legend Gears Legend
Gears Legend

Get an Answer from our SE Support, for the SE 8 Viewers and SE8.

After install from SE8 or SE 8 Viewer (Insight Connect), install also MP 01.

Have test this was working after I run again the iSeriesInstall.bat.

This solved the problem with JT2Go and SE8, SE 8 Viewer, or Insight Connect.

 

 

 

Re: How to Install JT2Go 10 and Solid Edge ST 6 at the same Computer with no conflicts and crashes?

Valued Contributor
Valued Contributor
It is solved also with JT2Go version 11 64 bit because it use other Reg Keys.
You need only for JT2Go version 10 32 bit the procedure like known with the iSeriesInstall.bat.