Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add custom property or change it for many files at once?

Pioneer
Pioneer

Hello

 

How to add custom property or change it  for many files at once? 

Files are not inside assembly and I dont want to add/change status from the level of Property Menager.

I've many files on my drive and want to add to it some custom property.

Of course I can do this from Property Manager. But to do this I would have to put all parts to assembly environment ( which will taka a lot of time).

So, is  it possible to do this from windows explorel level? Or maybe there is some additional tool to do this?

Or maybe there is possiblility to put multiple files to assembly file. If so, I could do it from the level of Property Menager or Project Menager.

 

Regards

2 REPLIES 2

Betreff: How to add custom property or change it for many files at once?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SUCHY

 

 

this is not completely true!

 

You can use the Property Manager without any assembly too.

Just start it from teh Solid Edge button and go to the folder, select all files and change the props.

 

20180328_1021.PNG20180328_1023.PNG

 

 

regards
Wolfgang

Betreff: How to add custom property or change it for many files at once?

Pioneer
Pioneer

Thanks Wolfgnag. This sollution is ok for me.

 

Regards