Cancel
Showing results for 
Search instead for 
Did you mean: 

How to add manually created parts into solid edge standard parts library

Experimenter
Experimenter

i would like to add some of the parts (which is created manually) into the solid edge standard parts library, some one kindly help me to do this.

 

- Maheshwaran 

5 REPLIES

Re: How to add manually created parts into solid edge standard parts library

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

First of all, I suggest reading StandardPartsUserGuide.chm (c:\Program Files\Solid Edge ST8\Program\ResDLLs\0009\), because it contains info what you need for.

 

And here is a video about steps:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: How to add manually created parts into solid edge standard parts library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics,

Thanks for that. No documentation I've seen made any sense to me. Your video does.

I never knew that add from existing part meant that it had to be open in SE.

Now, we are using Insight and our standard parts are on a sequel server. Will added parts go there as well?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: How to add manually created parts into solid edge standard parts library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics,

I added a part (hilited) to the standard parts library but it doesn't display in the application.

Any ideas?stdpartaddition.PNG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: How to add manually created parts into solid edge standard parts library

Gears Phenom Gears Phenom
Gears Phenom

@bshand did you try to create a new category and add to it?

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: How to add manually created parts into solid edge standard parts library

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I didn't. I used an existing, native, category. I take it that it is necessary to create a new category even if the part really belongs in the same category? That would mean that the user will have to know to go to another category. One wonders why.

 

My example involves a bolt which is fully threaded. Full threaded 1-8 unc X 5" bolts are not available in the library but they are available in the real world. And we needed one. So I copied the standard one out, made it full thd, renamed it, and attempted to add it back in thinking it would show up next to the standard one.

Nope. Administrator can see it but not in the regular interface.

 

I'll give it another go when I get a chance. Don't like this tool. Never did.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200