Cancel
Showing results for 
Search instead for 
Did you mean: 

How to center features in Sheet Metal?

Builder
Builder

This one is borderline embarrassing... http://screencast-o-matic.com/watch/cIjqlvVk1R

 

I can't seem to figure out how to center features to other features. I figured the symmetry face relate would do it, but it doesn't seem to work for this application. I could use dimensions, but they wont scale properly as I edit the rest of the part.

 

Thanks again

3 REPLIES

Luke,   Have a look at this video and see if it helps.  h...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Luke,

 

Have a look at this video and see if it helps.  http://screencast.com/t/KEmRGIyvu4G

 

You can create face relate relationships to honor the conditions you want.

Note that you do not need to create "all"  the relations becasue live rules still "finds" the coplanar by axis.

 

HTH

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

Re: Luke,   Have a look at this video and see if it helps.  h...

Builder
Builder
http://screencast-o-matic.com/watch/cIjqIAVkiE

Maybe it's not working because it's a patterned feature?

Re: Luke,   Have a look at this video and see if it helps.  h...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
yea, that makes sense. The Pattern is a procedural feature...

You could drop the pattern and constrain as shown
or
reset the pattern origin to the plane of symmetry.
Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/