Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create Draft Angle in Surfacing

Phenom
Phenom

Hi,

 

just wondering if someone of you know how to create surface with draft angle to adjacent surface ?

 

How to do this using commands from Surfacing ?

 

Thank you,

 

Regards,

 

Arek


Production: SE ST10 MP8
;
3 REPLIES

Betreff: How to create Draft Angle in Surfacing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

 

there are 2 questions/hints  I have:

 

  • why do You us surface ?
    Would it be possible to do the same using body design?
  • If surfaces must be, then You should use the "Rule Surface" command.
    There You can define a draft angle (and more),
    but You would get a new surface rather than a modified original one.

 



regards
Wolfgang

Betreff: How to create Draft Angle in Surfacing

Phenom
Phenom
@Howcad

Hi,

Thank you Wolfgang.

I know how to do it using body design - still learning surfacing hence my question.
I know there are a lot of tricks , different methods to do something.

Regards,
Arek

Production: SE ST10 MP8
;

Betreff: How to create Draft Angle in Surfacing

MLombard
Retired

@arekkul

This is a good question. In practice, what I typically do is get the thing solid, then add draft, or add draft as part of modeling the surfaces, depending on the part. I do believe that this is one area where Solid Edge needs some improved functionality. I would say an enhancement request would be in order to enable draft on surfaces.

Retired Community Manager for Solid Edge. This account is no longer active.