Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to create border in Solid Edge Electrical

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Solid Edge Electrical comes with some predefine border. But how new custom border & properties/attribute can be created.

6 REPLIES 6

Re: How to create border in Solid Edge Electrical

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Your question is very general so I will answer very generally.

You can modify the existing border or create new ones on the background sheets. Insert callouts or text with the desired properties.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How to create border in Solid Edge Electrical

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thanks for Reply.

But I require this in solid edge electrical module, not in solidedge draft.

Re: How to create border in Solid Edge Electrical

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Krunal I doubt too many here are running SE Electrical which is basically Mentor Graphics, and there is no Mentor Graphics forums in the Community yet.  You may have to consult support or the documentation to get your answer.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: How to create border in Solid Edge Electrical

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So I've clearly revealed my complete ignorance of SE Electrical. Yet another subject on which I'm lacking know-how.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How to create border in Solid Edge Electrical

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

You can creat a new border on Solid Edge Eletrical Symbols that comes with the Solid Edge Eletrical Design.

View the image that a sent2019-05-03 09_54_13-Solid Edge Electrical Symbol.jpg

 

 

Re: How to create border in Solid Edge Electrical

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Krunal,

 

Adding more to f_silva's reply. 

 

You can use existing border library and create a new border inside it. See the image:

New border creation.JPG

 

Also launch help from Solid Edge Electrical Symbol application. You would find relevant info in chapter ' Border Drawings'.