Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create chart drawing (Single draft file) for multiple assemblies

Experimenter
Experimenter

Dear Solid Edge Users,

I have multiple assembly files which are very much similar to each other. These assemblies are created using family of parts. In case of family of parts, we can create single draft file for multiple parts.

Similarly, I want to create chart drawing (single draft file) for multiple assembly files. I don’t find any such option in solidedge.

Is there any such command or option so that I can create single chart drawing (single draft file) for multiple assembly files? Please advice.

 

Thanks, Jayawant Kamble (jayawant.kamble@gmail.com)

2 REPLIES 2

Re: How to create chart drawing (Single draft file) for multiple assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's not clear what you are asking. What is a "chart" drawing? What do you want the assemblies to do in the draft file?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: How to create chart drawing (Single draft file) for multiple assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @jkamble

 

 

 

if Your question goes in the direction of a "Family Of Assemblies Drawing" like it is with the "Family Of Parts" drawing inclusive the dimension table, then the asnwer is IMHO a clearly NO

 

 

If the draft should show the position of alternating positions then YEs, You can do that.

 

regards
Wolfgang