Cancel
Showing results for 
Search instead for 
Did you mean: 

How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
9 REPLIES

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is that in the base product or is it a paid add-on and how much does the add-on cost?

 

I don't know of anything in the base Solid Edge product that will do that automatically.  You would have to build it manually.  May be a 3rd party add-on to do it but not sure.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Valued Contributor
Valued Contributor

Would this be possible in ST9 using the new solid tooling path tool (I'm sure it has a better name)?  The opposite roller would be mirrored looking at the example.

 

Edit: Solid Sweep....

 

https://www.youtube.com/watch?v=813owZBoLUs

 

 

Guy



CAD/CAE Manager
ST8 MP9

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Phenom
Phenom

Here's how something like that is done in NX.

 

This was an interesting demo of some advanced specialized tool. I don't think NX nor SE has the full suite of functionality that this demo is showing. I have no doubts that NX has all the tools to do what is shown but I don't think those tools are "packaged" into a point solution like TopSolid has done. And make no mistake this a custom point solution. But I will say, this solves some interesting problems but it also poses some interesting questions as well.

 

As a previous demo jock (quite awhile ago) it's the small things that matter the most. In this case the source was a facet or surfaced model and not a solid body. It would be interesting to see this happen with a solid body. Since this is a point solution, you can tell because the function is called timing screw, that this is only going to work with cyclindrical rollers since the demo didn't show any other application. The scenario file is the key here as it locates the position and oreintation of the source "body" and then a helixal path has to be built based on the inputs.

 

The animation was built on simulations and not part of the "specialize timing screw function". But all in all it is a great demonstration of what can be done when you can define a problem and then build custom coding around it.

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Solid Edge ST9 will provide a nice feature to this, its name is Solid sweep (cut).

 

Here is a short video:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Yes, this could be the solution in solidege ST9 but still if we see in topsolid AVI the pitch of helix cut goes on decreasing which allows to rotate bottle.

 

I guess, that is bit difficult to control it in solidedge that easily.

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Phenom
Phenom

Yes, the rotation of bottle is being driven by the scenario file and there is some serious cross sectional lofting happening to the trim surface used to cut away the path on the roller. That you aren't going to get with a single feature inside of any CAD system. Like I mentioned this is a point solution/ custom coding for Topsolid. I image with the right people something similar could be done in most CAD systems.

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

You can do this at this moment in SE, but you have to use Simply Motion...

 

Here is a video:

 

Yes, I know this is not an "one button solution" but works.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Valued Contributor
Valued Contributor

Hi, here is a screw I did with ST7 for a vaccum juice extractor.

The advance of the screw is constant. 1/4" every 5 °

But I think this method can be applicable to a non-constant advance.

 

Alex

 

untitled.289.jpg

 

Good Marketing makes the company look smart.
Great Marketing makes the customer feel smart.

Re: How to create timing fedder conveyer in solidedge. It can be very easily created in topsolid.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Yes, we can do this.

Thankyou...!!