Cancel
Showing results for 
Search instead for 
Did you mean: 

How to customize ribbons with commands?

Valued Contributor
Valued Contributor

Hello Experts,

 

Just after ST6 installation in the new laptop the upper ribbons with commands are grouped on tabs. Please see attachment 1 in black rectangle.

"Increase buttons on command ribbon 2X" is turned off.

 

I would like expand these ribbons more detailed - please see attach. 2. Where should I set it?

 

It runs on win 7 1920x1080 res.

 

Thanks a lot!

 

CB

3 REPLIES

Re: How to customize ribbons with commands?

Phenom
Phenom
It all depend by how wide your Solid Edge Windows is.
In picture 2 it is clear that is full 1920 wide, in picture 1 it look like a 1600 wide and there isn't enought space for all the buttons.

Easy way: increase the size of Solid Edge Window or better maximize it.

Another way: customize the ribbon and remove (or rename shorter) text from buttons that you don't often use (for example "Editor Struktury component" take a lot of space for no reason)

Re: How to customize ribbons with commands?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can also impact your button icon configuration and layout by changing the icon size and icon text display settings:

 

1. On the tool bars right-click --> 'Customize the Ribbon...'.

 

2. In the Customize dialog, in the right-hand pane right-click --> 'Button Options...'

 

3. In the Button Options dialog you can control the following:

 

'Size' --> 'Use only small buttons', ‘Use only large buttons’, or ‘Use only small buttons’

 

‘Text’ --> ‘Use text and no text buttons’, ‘Use text on all buttons’, or ‘ ‘Do not use any text on buttons’

 

4. Select 'OK'.

 

5. Select 'Close'.

 

6. When prompted, save your changes to a new Theme.

Re: How to customize ribbons with commands?

Valued Contributor
Valued Contributor

Dear Dave,

 

We did not know that, thank you! Everyone has forgotten mouse right button exists in SE options Smiley Wink