Cancel
Showing results for 
Search instead for 
Did you mean: 

How to design the crane hook.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I have attached the dimenion for the hook. I have used sweep command in part with multi-path and           multi-crossection option. I have completed the nearly 80% for work but the issue is at the end while making the dome shape part. Sweep doesn't work here.

4 REPLIES 4

Re: How to design the crane hook.

Gears Phenom Gears Phenom
Gears Phenom
Remember that you can use "dots" as swept section, if you use it at the end of the swept then change the "end condition" to tanget and increase it's value it will create a shape like the expected one.

Re: How to design the crane hook.

Gears Phenom Gears Phenom
Gears Phenom

@Fiorini wrote:
Remember that you can use "dots" as swept section, if you use it at the end of the swept then change the "end condition" to tanget and increase it's value it will create a shape like the expected one.

I just discovered that this doesn't work anymore. I'm on ST8 and I don't know when this broke out but it is a big loss of functionality.

Re: How to design the crane hook.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

I'm not sure if Swept had the point capability before but in ST9 and some versions before you can select a point in the surface patch command.

This command also support a "guide curve" so you can use the curve you have in a sketch corresponding to your Elevation view in your image. (see the image attached, i'm not very clear in my explanation !)

With curvature continuous, the result is pretty good.

 

For the swept feature, i used the Arc lenght options so the two sides of the swept are followed until the end. I'm not sure about the exact shape of the hook though...

 

 

 

Nicolas Bernard, Application Engineer, Solid Edge French Resseller

Re: How to design the crane hook.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Its working wih bound. Thank You...