Cancel
Showing results for 
Search instead for 
Did you mean: 

How to display Chinese characters

Not applicable

Hi, I am using a operating system in English version, and installed the solid edge
2D software in Chinese vesion, because I'd like to add some notes in Chinese, however
the solid edge can not display the Chinese character properly. So do you have a
solution for this kind question?
Thanks a million!

4 REPLIES

Re: How to display Chinese characters

Not applicable
Shawn,
You can try changing the language settings on the machine.
Regards,
Rick B.

non unicode

Not applicable
I've installed the russian version of SE 2D and it doesn't display characters properly. Sistem local for non unicode programs is set "russian". Windows 7 is running english. Other programs with russian versions work properly. Is the any solution for this problem ?

[langtitle=ru]Re: non unicode[/langtitle]

Experimenter
Experimenter
i've installed the russian version of se 2d and it doesn't display characters properly. Sistem local for non unicode programs is set "russian". Windows 7 is running english. Other programs with russian versions work properly. Is the any solution for this problem ?

Я использую ГОСТовский шрифт от Компаса. :-)
Не совсем лицензионное решение, тем не менее ничего лучше пока не придумал.
Надеюсь, в новой версии двухмерного Солида поправят эти косяки.

Re: How to display Chinese characters

Not applicable
Solid Edge 2D Drafting ST3 will be released soon. It supports Unicode.
It will allow character sets from diferent locals to dbe displayed.
I will post a message to the newsgroup when it is available for download.
Regards,
Rick B.