Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to display views saved in model?

Genius
Genius

How do I look at and / or modify model views that have been setup in a model previously using the PMI - Model Views - View command?

ST10 MP9

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Commercial & Residential Solutions | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

3 REPLIES 3

Re: How to display views saved in model?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Seems like you can only apply it via the view wizard on a new view.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How to display views saved in model?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Gary,

 

Within the model itself they get listed in the PathFinder under the PMI node:

 

GDPMIView01.png

 

Right-click on each of those view nodes to bring up a context menu that has commands for editing/redefining the view using the same dialog that you used for defining it in the first place.

  

And as Bruce has suggested, it is available in the Drawing View wizard or much later after the view has been placed, under the Drawing View Properties (see the bottom-right corner of the dialog):

 

GDPMIView02.png

 

~Tushar

 

 

Re: How to display views saved in model?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Aha! I was surprised I couldn't find a way after a view was placed. Didn't think to look in that area nor did I see anything like that in help. No surprise there I guess.

I'll take that back, I do see it in help now.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200