Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to do skeleton modelling in solidedge.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

w

6 REPLIES 6

Re: How to do skeleton modelling in solidedge.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In order to even approach your question we're going to need more than a skeleton posting.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How to do skeleton modelling in solidedge.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Skeleton modelling is same as top down assembly. Consider an example of OEM company, they outsource there design to their venders on basis of co-ordinate system same as carline concept. So when they get there design back they pull all parts in assembly and it will automatically get assembled according to coordinate system even without applying assembly constrains. This can be done very easily in NX

 

Please go through the below link which showcase skeleton modelling in inventor.

https://youtu.be/uC3ia17t48c

Re: How to do skeleton modelling in solidedge.

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm not familiar enough with them to know for sure, but it seems like Virtual Components would be the closest equivalent in Solid Edge.

 

Greg

Re: How to do skeleton modelling in solidedge.

Phenom
Phenom

@Krunal yea we work in a very similar way to the video you linked to, with a master sketch in an assembly that drives the parts below it - we use it for sheet metal welded assemblies where individual folded plates are built up to make complex 3D structures.  

 

Try drawing the sketch in the assembly, doing "create part in place" then use the "copy sketch" function to copy that sketch into the part file where it will retain the associative link - note this works in ordered mode only unfortunately.

Re: How to do skeleton modelling in solidedge.

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you...!!!

 

Will try and update you.

Re: How to do skeleton modelling in solidedge.

Honored Contributor
Honored Contributor

I have found that most of the time it's easier to create a series of 2D sketches on planes rather than use 3D sketches. So the first step is creating planes where the work needs to be done. Since frame design is Ordered/Assembly mode only, and is the most common use of wire frame design, I would start with an assembly file and 2D assembly sketches on planes.

 

I would only use a 3D sketch if it was really necessary.