Cancel
Showing results for 
Search instead for 
Did you mean: 

How to export Solid Edge data out of Sharepoint without loosing links?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Bugetary constraints are limiting my customer's ability to upgrade and so the conclusion is to get rid of Sharepoint.

 

My question is how to export Solid Edge data from Sharepoint into native Windows without loosing any links?

 

 

2 REPLIES

Re: How to export Solid Edge data out of Sharepoint without loosing links?

Hello Gary,

Are you referring to Solid Edge Insight or Solid Edge for SharePoint?

Regards,
Theodore
Kind regards,
Theodore Turner

Re: How to export Solid Edge data out of Sharepoint without loosing links?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If talking about Insight, I am using RoboCopy to bulk export files out of SharePoint using the webdav path for the source file.

 

Now in regards to preserving links, they should still work given that no one renamed files in Insight without updating the various files that may have referenced them.

 

One thing to note is that Solid Edge flips the internal SE security flag on the files to read only when it stores the file in SharePoint and it stays that way when you export it so you will need to run a status changer on all of your files that you want writeable.  If their status is to stay as Released or Obsolete then you can skip those.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com