Cancel
Showing results for 
Search instead for 
Did you mean: 

How to extrude a 2D DXF drawing

Creator
Creator

Hi all, I'm new to ST10 and 3D modelling in general, although I have used several 2D packages...

 

The question is, I imported a 2D drawing from a DXF file. Drawing consists of lines and arcs making a closed region.

Now I want to extrude that region and create a 10mm thick part with that shape.

 

However, when I try to extrude it, I get it to "rise", but then I get this error:

 

"Base features require closed profiles. This feature's profile has become an open profile."

 

What is missing ?

 

26 REPLIES

Re: How to extrude a 2D DXF drawing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Your profile seems to be closed, but probably the entities are NOT connected.

You may check, whether the end points of each entity (line, arc) have a Connect relations (little square around it while displaying the profile relations).

Sketch.png

Re: How to extrude a 2D DXF drawing

Creator
Creator

No. When I do that, I only get little red dots.

So, how do I connect them ?

 

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @pjrebordao

 

 

 

when You use the 3D Create command from a draft file (where You imported the DWG, then You should find Your sketch in an e.g. part document as a sketch with a sketch region.

Tip: use a synchronous part therefroe.

 

Click onto the region and use the white arrow to pull the region to 10mm thickness

 

 

You can clean up teh sketch before in draft to automatically connect those entities correctly

as mentioned by @MartinBernhard

 

 

regards
Wolfgang

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @pjrebordao

 

 

 

just did a search for "Solid Edge Youtube Create 3D" and found this video as first of several

 

https://www.youtube.com/watch?v=RHj2ozmj4zw

 

 

regards
Wolfgang

Re: How to extrude a 2D DXF drawing

Creator
Creator

I tried your ideas but I think i have an underlying problem.

In my DXF, the lines and arcs are probably not connected (although they end and start at the same point), so I can't never grab the "whole" as a region.

So, how to connect them ?

 

 

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @pjrebordao

 

 

as said before, if the are in the correct size this should be now further problem when working synchronous, as long as the can build an closed region.

 

But or better and You also can repair/optimize those 2D geometry using the  "Relationship Assistant"

 

20171117_1951.PNG

regards
Wolfgang

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @pjrebordao

 

 

 

I have forgotten to mention that if You start the assistant once and press the help button YOu will come to not so bad, or better se good help page showing hhow it works.

 

 

regards
Wolfgang

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

IMO often the simplest way, depending on the type of geometry, to make sure it's closed is to use the trim corner function.

trimcorner.JPG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: How to extrude a 2D DXF drawing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I just opened a new st10 part. In sync I opened a simple square shape in a sketch, picked the region and it wouldn't extrude. I'm surprised. I could add a video but gotta go. Could this be what's happening to the novus OP?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200