Cancel
Showing results for 
Search instead for 
Did you mean: 

How to extrude only one side?

Honored Contributor
Honored Contributor

There is another thread with exactly the same question, but the vid answer is not available.

 

Here was the question from another thread:

 

I use Extrude command to make object on the surface of another object, and after I draw the profile on the surface and accept, they request to choose "non-symetric extent" or "symetric extent", and "through all", "through next", "from/to extent" or "finite extent".

But after I choose one side and enter the dimension, they ask me to enter the dimension of opposite side. But I don't need the opposite side.

So how can I choose only one side to make prominent object?

 

 

1 REPLY

Re: How to extrude only one side?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I can only assume that you are using Ordered modelling. In which case it would appear that you have at some time previously set the command bar to Extrude - Non symetric extent. As these commands are modal it will remain set what ever way you last used it.

ext1.JPG

In this case the the Non-symetric extent is highlighted.

To 'fix" this issue simply click on the highlighted icon and it will return to the simple extent mode.

 

Cheers

Mark