04-13-2016 07:08 AM
Hello all.
I have a problem in dimension in Solidedge ST3 like a figure below..please have anyone idea?
How to remove this suffix -3 Places.
Solved! Go to Solution.
04-13-2016 07:25 AM
04-13-2016 08:08 AM
04-13-2016 08:11 AM
When placeing the next dim, don't place it. go up to modify prefix and clear the box's. this should clear the default
04-13-2016 08:39 AM
04-13-2016 08:49 AM
take a look at this http://www.screencast.com/t/JtMT85MF
04-13-2016 09:09 AM
04-13-2016 09:41 AM
04-13-2016 10:13 AM
The SmartDimension CommandBar should appear when you click on Smart Dimension tool. If that's not happening, it might be in a collapsed panel on the side of the screen or it may have been moved off of the screen. You might try going to Solid Edge Options>Helpers>Command User Interface, and switching to either Use Horizontal Toolbar Form or Use Vertical Docking Window Form, and see if that resolves the problem. If not, there is a registry key you can use to clear the interface that will set it back to default. Or, you could use one of the pre-set Themes.
If you change the theme to Some Assistance or Maximum Assistance, it will rearrange your interface. It may be a good idea so save your current interface as a theme in case you want to return to it.
04-13-2016 10:32 AM - edited 04-13-2016 10:33 AM
Thank you ,Thank you.. TDB.