Cancel
Showing results for 
Search instead for 
Did you mean: 

How to flip direction of a circular pattern?

Pioneer
Pioneer

Pretty simple question I think...After I've already created a circular pattern, how do I flip the direction (CW vs. CCW)?  The "Flip" button has to do with suppression region occurences.

Reason would be if I'm only doing a partial circle.

sryp

ST7 Classic MP0 | Win7
3 REPLIES 3

Re: How to flip direction of a circular pattern?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @sryp,

 

That "direction" step is consumed after placement......just re-do it, and make your direction [opposite] as desired.

Not ideal, I know....this would be a good ER [Ehancement Request], to your VAR or to GTAC, if you have direct access that way.

 

Alternatively, you could use a pattern "Along Curve", and re-define that as much as you like, after the fact.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: How to flip direction of a circular pattern?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Probably easiest is in the sketch profile step, use the Mirror element command (make sure to turn Copy option off) to mirror the other way.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: How to flip direction of a circular pattern?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Oh yeah, @KennyG is spot on...I forgot about being able to modify the pattern sketch.

 

Something about, not seeing the wood, for all the trees.... Robot wink

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000