Cancel
Showing results for 
Search instead for 
Did you mean: 

How to increase a frame length in assembly

Pioneer
Pioneer

Dear sir ;

       I need your help. How to increase the frame length in assembly model. if you have any video link please sent't me 

    

4 REPLIES
Highlighted

Re: How to increase a frame length in assembly

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

The easiest way is to start with a sketch and put the required relationships and dimensions on there.  However if you have already created the frame you can attach dimensions to the individual frame elements.  You can then simply edit these by clicking on them and changing the value.  Alternatively you can define a formula for any of the dimensions to be related to one.  Enter a formula by double clicking on the dimension as shown in this video:

 

http://www.youtube.com/watch?v=cteAKYPTgDc&feature=youtube_gdata

 

Hope that helps,

 

Frank

Edinburgh University

Re: How to increase a frame length in assembly

PLM World Member Genius PLM World Member Genius
PLM World Member Genius
I think there is even a quicker way...if it still works in ST7. Double click the dimension you want to be driven and then single click on the driving dimension and hit enter. This automatically builds the link you were showing via manual input. Repeat for the other two dimensions and you're done.
--
Ryan Gudorf
CAD/CAM Supervisor
Budde Sheet Metal Works, Inc.
Windows 7 Professional x64 SP1
Solid Edge V20
NX11.0.1
TC10.1.5 32 GB RAM, nVIDIA Quadro K4200

Re: How to increase a frame length in assembly

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
You're right, that is quicker and it does still work in ST7.
Edinburgh University

Re: How to increase a frame length in assembly

Pioneer
Pioneer
hi:
Frankmill i am happy very use full for given a solution

Thanks&regard
ANAND.G