Cancel
Showing results for 
Search instead for 
Did you mean: 

How to know if a part in the assembly is a member of family part?

Experimenter
Experimenter

If a family member is used in an assembly, how can I know it is a member of family and also how can I know what the family template is?

For example, family part SE20150824.par have two members of SE20150824-01 and SE20150824-01.

When  SE20150824-01 is used in SE20150824A01.sam, How can I get the relationship from SE20150824-01 to SE20150824.par using  c# API?

 

1 REPLY

Re: How to know if a part in the assembly is a member of family part?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi kanwal:

 

Post this in the Solid Edge Development Forum.

 

~Tushar Suradkar

www.SurfAndCode.in