Cancel
Showing results for 
Search instead for 
Did you mean: 

How to make a copy of a part/assembly?

Valued Contributor
Valued Contributor

Hi,

 

I make make a simple frame (50x50) with some holes in each end.

The frame/tube is made within an assembly.

 

I now need to make a copy of the file.

The only difference between the two files will be the length of the tube, the new one need to a bit longer.

 

How can I copy the file? So I can do the adjustment in the new file/assembly.

The new assembly must not make a copy of the 50x50 tube-template.

 

I guess I need to use Design Manager, but not sure what buttons to use to make a copy of the assembly.

 

Hope one of you might be able to help me Smiley Happy

 

 

Thanks,

 

 

2 REPLIES

Betreff: How to make a copy of a part/assembly?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

 

if - as You mentioned - there are only frames within Your assembly, then a simply "Save As" will do it.

 

 

But going to the Data Management tab will let You allow also to "Save As" and same is true for the Design Manager

 



regards
Wolfgang

Betreff: How to make a copy of a part/assembly?

Valued Contributor
Valued Contributor

Awesome, will try that Save As function then.

Update: Worked perfectly.

 

Thanks and merry Christmas Smiley Happy