10-15-2015 04:16 AM
Hi,
I have 4 holes in a sheet metal place and would like the distance between the holes to be equal. How is that possible?
10-15-2015 04:59 AM - edited 10-15-2015 05:06 AM
Hole Pattern as you can do fill so will be equal or Locked Dimensions and Formula for the holes
10-15-2015 05:00 AM
Hi,
I would use a pattern here.
Think this is the easiest method to bring equal distance bewteen those 4 holes, isn't it?
10-15-2015 11:02 AM
I draw 3 lines between the points and make the lines "equal". (= sign)
This is in ordered.
10-15-2015 11:25 AM
In either mode, if you don't want to use a pattern, you can use @ChrisMorgan's 2nd solution of dimensions with formulas. I would just make two of the dimensions equal to one of them or make each dimension equal to 1/3 the overall.
10-15-2015 02:38 PM
I use joris' method alot or else I make a pattern in a sketch first and then pin the hole to that sketch. Then pattern the hole from the sketch.