Cancel
Showing results for 
Search instead for 
Did you mean: 

How to make this relation?

Phenom
Phenom

This is something we do in real life, but I can't achieve this in SE...

Any idea how to make a correct relationship between these two parts?

fix.png

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
3 REPLIES 3

Re: How to make this relation?

Gears Phenom Gears Phenom
Gears Phenom

Connect relationship betwhen screw cone and hole edge.

 

 

Re: How to make this relation?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Joris,

 

The easiest way is to use the connect relationship. For the face on the screw, use QuickPick to select Cone (Protrusion 1). For the face on the base, use QuickPick to select Edge (Hole 1) from the top of the inner diameter of the hole. I have attached the example with the relationship created.

 

Hope this helps,

Greg

 

Edit - looks like two of us were working on it at the same time

Re: How to make this relation?

Phenom
Phenom

Of course...

Thanks for your effort both. ;-)

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user