Cancel
Showing results for 
Search instead for 
Did you mean: 

How to merg solid body with surfaces to create one whole body?

Builder
Builder

Hi Folks,

 

I have this body that had a extrusion on the wrong side so I mirrored it. The result is a body with the the correct extrusion direction but I want the whole thing to be one solid body. How can I go about doing this?

 

Thanks

3 REPLIES 3

Re: How to merg solid body with surfaces to create one whole body?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In a new par or psm use "insert part copy"?

I had to reduce the diameter of the hole in the main part so I could attach the toroidal mirror feature before part copying it. Otherwise that feature wouldn't be in the new part.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: How to merg solid body with surfaces to create one whole body?

Builder
Builder

Could you upload that file differently as I am on st7?

Highlighted

Re: How to merg solid body with surfaces to create one whole body?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For some reason I couldn't attach a step file. I had to zip it.

 

Edit: You should optimize it after opening.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200